InfraStruXure InRow RC
Row based, chilled water cooling solutions for medium to large data centers including high density applications.
Data center heat densities continue to increase, making it more difficult to provide adequate cooling. To ensure proper airflow paths the distance between the heat source and heat removal system must decrease. The InRow® product design closely couples cooling with heat load, preventing exhaust air recirculation to sensitive IT equipment. The InRow RC is a computer room chilled water cooling system designed for installation in the row to maximize sensible cooling and increase efficiency. The unit captures heat directly from the hot aisle and distributes cool air ensuring that equipment temperatures are constantly held to setpoint conditions. The energy-efficient design lowers total cost of ownership by monitoring IT equipment inlet temperatures to modulate capacity based on the demand for cooling. Fan speed is controlled based on the demand to reduce energy consumption during off-peak cooling periods. Heat rejection for the unit can be handled through an existing chilled water system or an APC supplied chiller. The modular, scalable solution improves agility by enabling you to add cooling as demand increases, making the InRow RC ideal for small to large datacenters.